המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to upload a Ecostruxure Power Commission project (pcet )to the cloud?
1. Launch the Ecostruxure Power Commission desktop application.
Application Icon

2. The user is displayed the list of available projects in the Ecostruxure Power Commission application ( as shown below ) Note: Switch to classic view is enabled
Project list view in classic view

3. Click on the "upload to cloud" symbol of the project as shown below
Uploading the pcet file to cloud

4. The project will be successfully uploaded to the cloud and the user can view in the project list with the last backup details of the project
information/details of last update to the cloud