המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why OFS 3.63 SP3 has some start-up latency or doesn’t start?
The OFS 3.63 SP3 has integrated some CRLs access from Internet.
However, in certain condition of used, OFS can be installed on a computer where no internet connection is available.
Therefor, OFS won’t start or start with a long period of wait.
To avoid this, the proposed workaround is to bypass this step of the online CRLs access by modifying a registry key.
To do it, the value of the following registry need to be modified either using the “SetReg” tool proposed by Microsoft or manually by accessing to the registry.
  • Using SetReg by Microsoft:

The SetReg tool give the following information:
SetReg Tool 1

The parameter 3) need to be changed from TRUE to FALSE as followed by executing the following command : SetReg 3 FALSE

SetReg Tool 2
  • Modifying the registry key manually:
The involved registry key is the DWORD State key under :

KEY_CURRENT_USER\SOFTWARE\Microsoft\Windows\CurrentVersion\WinTrust\Trust Providers\Software Publishing

This is the Key registry for the current user. If your OFS is launched by a specific user, please do the same on this specific user registry key.

State valueSetReg commandEffect
0x00023e00SetReg 3 FALSEDisable CRLs online access
0x00023c00 (default)SetReg 3 TRUEEnable CRLs online access

Registry

This issue will be corrected in the next release of OFS.
  1. Product Line
OFS 3.63 SP3
  1. Environment
Windows 10, Windows Server 2022