המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What does RF CAL mean on my Accutech base radio or field unit?

RF CAL message on the Accutech base radio or field unit indicates that the radio is out of calibration. This could be because the radio has lost it's RF calibration data or that the RF frequencies have drifted over time and are no longer within specs.

If a device is showing "RF CAL" and is not communicating properly, there isn't anything that can be done in the field. The Accutech device will either need to be replaced or repaired.

In Canada and the United States, please reach out to the Foxboro Repair Center at svcusfox.repairs@se.com

For overseas, please reach out to your Schneider sales representative for further assistance.