המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Are APC Back-UPS and Smart-UPS Medical Grade?

Issue:
Are APC Back-UPS and Smart-UPS considered medical grade?

Product Line:

  • All Back-UPS models
  • All Smart-UPS models
  • All Serial Numbers

Environment:
Healthcare facilities and medical environments where equipment requires reliable power protection.

Cause:
Medical-grade power protection devices must meet specific safety and performance standards to ensure they are suitable for use in healthcare settings.

Resolution:
APC Back-UPS and Smart-UPS products are not classified as medical-grade devices. While they provide reliable power protection primarily intended for IT Equipment (such as computers, networking devices, routers, switches, telecom, etc.), they do not meet the strict requirements set by regulatory authorities for medical equipment. For medical applications, it is recommended to use UPS systems that are specifically designed and certified for medical use to ensure compliance with safety and performance standards.