המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the .zdat file from Vijeo Designer used for?

Issue:

.zdat file extension from Vijeo Designer


Product Line:

Vijeo Designer, EcoStruxure Operator Terminal Expert


Resolution:

The .zdat file is exported from Vijeo Designer software as shown below and is used for converting the Vijeo Designer project to EcoStruxure Operator Terminal Expert project. The .zdat needs to be inputted into the Migration tool

Note: The Migration tool to migrate from VJD to EOTE has been put on hold temporarily

image1

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר: