המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to Extract Data in SBUS server?

Title

How to extract data using SBUS server?

Issue

Data is needed outside of EPAS application, for example, technical analysis, reporting, data archival, etc.

Product Line

EcoStruxure Power Automation System (EPAS)

EcoStruxure Microgrid Operation (EMO)

PACiS

EcoSUI

Environment

SBUS Server

Resolution

  1. Open SBUS server application > select the Extraction tab
  2. Select measurements to be extracted by either:
    1. Selecting individually using the Select Signals window (click save to create a .lst file for repetitive use)
    2. Select 'Load' to import a list file (.lst)
  3. Select dates for the desired time period > Extract. NOTE: Depending on dates selected and number of signals, files can be quite large.

SBUS server extraction

4. Select the directory where you'd like to store the extraction file and select Save.