המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is Multilanguages Online Help Available in Control Expert v16.2 ?

Issue: The Control Expert v16.2 online help is delivered in English for all GUI languages. Some customers want a translation of the Control Expert Online Help into other languages.

Product Line: EcoStruxure Control Expert

Environment: EcoStruxure Control Expert v16.2

Resolution: To support better usage in other countries, translated versions of the online help are provided in French, Italian, German, Spanish, and Chinese in Control Expert v16.2. The customer does not need to install a Hotfix. The multilingual feature is integrated into the v16.2 setup.