המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ETE - FAQ - Transformer: What are the possible causes of failure in a transformer?

The main causes of failure in a transformer result from a compromise of the internal insulation. This results from the cumulative effects of aging, mechanical damage or, in some circumstances, design or manufacturing faults.

Insulation within most transformers is essentially paper impregnated with oil. This insulation can be compromised during the transformer's life by mechanical stress (vibration) or certain aging processes degrading the paper and the oil. These processes are well understood by Schneider Electric.