המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ETE - FAQ - Offer: Will the use of the EcoStruxure Transformer Expert solution increase the life of a transformer?

The intelligence obtained from the EcoStruxure Transformer Expert solution can be used to plan optimum maintenance of transformers which will certainly increase transformer life.

  • At the early stage of life, the degradation of the transformer due to under-design can be identified.
  • During the middle phase, the EcoStruxure Transformer Expert analysis can be used to determine optimum operating conditions.
  • Towards the end of life, the analysis can be used to optimize end-of-life planning based on the actual health of the insulation, rather than nameplate age, as is often the case.