המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
M221 with Ecostruxure Machine Expert Basic - Always ON and Always Off Bits.

Issue:

Using EcoStructure Machine Expert Basic to program M221 PLCs in ladder logic, are there Always On and Always Off Memory Bits from the System bits (%S) that could be used?

Product Line:

EcoStructure Machine Expert Basic (all versions)

TM221 controllers

Resolution:

From the Machine Expert Basic help, there are no system bits (%S) listed for Always ON and Always OFF.

EME Basic Help

But in ladder logic it is easy way to program an Always ON and an Always OFF bits using normal memory bits (%M). See screenshot below.

Logic always On or Off.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)