המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to Migrate PME to a New Database Server

Issue

Migrating PME to a new database server.

Product Line

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Power Monitoring Expert

SQL Server

Resolution

  1. Confirm SQL server instance is compatible with the PME version by checking the corresponding system guide underneath Operating Environment. The link here will take you to the PME 2024 compatibility list: Operating Environment
  2. Follow the directions for a SBS upgrade for distributed systems. Ignore step 8. Step 2 - Transfer the Configuration
  3. Now that an archive has been taken, a system key has been generated and the databases have been transferred, the old version of PME must be uninstalled. Follow the instructions in the article "How to uninstall Power Monitoring Expert (PME) | Schneider Electric USA ". Do NOT skip steps as a clean uninstall is crucial to a successful migration.
  4. Install the new version of PME as a distributed system, pointing to the new database server. Installing the PME software
  5. After successful installation, detach and delete the freshly installed databases. Restore the old database backups.
  6. Open the CMTool, Load from Archive, and Write to System. Resolve any errors that you encounter.
  7. After a successful write to system, reconfigure the PME system.