המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Powerlogic P7 - No Voltage Display Using Open Delta PT Scheme and 52A signal Not Responding

Article available in these languages: Spanish

Issue:

The customer reports that voltages are not displayed and the 52B input status is missing on the mimic panel.

Product:

PowerLogic P7 Relay

Environment:

Relay configured with an Open Delta PT scheme and local HMI mimic panel enabled.

Cause:

The mimic configuration was not properly updated to reflect the PT scheme and input status, causing the local HMI to show incomplete or incorrect data.

Resolution:

Update the mimic configuration to ensure the local HMI is properly animated. Below are the recommended settings and layout adjustments:

1

2