המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why does EcoStruxure Control Expert v16.2 use the predefined custom path by default ?

1. Issue

Starting from Control Expert v16.2, the predefined custom path is used for operations such as Open, Save and Export, because the “Use defined custom path” option is enabled by default.
This feature, available under Tools → Options → Paths, was introduced to ensure consistency and prevent accidental saves in unintended directories.
In previous versions (16.0 and 15.x), this option was not functioning as intended, and the software always used the last opened path instead.

2. Product Line

EcoStruxure Control Expert v16.2.

3. Resolution

To restore the previous behavior (using the last opened path):

  • Go to Tools → Options → Paths.
  • Uncheck “Use defined custom path.”

Keeping the option checked ensures the software always uses the predefined custom path.

Use defined custom path