המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to generate a list of DNP3 Generic or Modbus - Advanced Generic Direct Outstations with their IP Addresses - Single Network

It might be helpful, for maintenance purposes, to have a list of outstations with their respective IP Addresses. Below are two queries that can be used to generate such lists for DNP3 Generic points and Modbus – Advanced Generic Direct Outstations, respectively:

SELECT

O.ID, O.FULLNAME, N.ADDRESS

FROM

CDNP3OSDIRECT AS O CROSS JOIN CSINGLENETWORK AS N

WHERE

O.ID = N.ID

ORDER BY

"FullName" ASC

-----------------------------------------------

SELECT

O.ID, O.FULLNAME, N.ADDRESS

FROM

CGENERICMODBUSOSDIRECT AS O CROSS JOIN CSINGLENETWORK AS N

WHERE

O.ID = N.ID

ORDER BY

"FullName" ASC

Please note that similar queries can be used to generate lists for other drivers. Proper tables for each driver can be found by using the Database Schema. More information on how to use the Database Schema can be found int the manual.

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר: