המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Project conversion from Vijeo Designer to Vijeo Designer Basic

-> Issue:

Convert a project from Vijeo Designer to Vijeo Designer Basic

-> Product Line:

HMI

-> Resolution:

It is not directly possible to convert a project from Vijeo Designer to Vijeo Designer Basic. These two platforms, while similar in name, are not fully compatible with each other. Vijeo Designer Basic is a simplified version of Vijeo Designer, intended for use with specific HMI models (like the Schneider Electric HMIGXU series), and it lacks many of the advanced features and drivers available in the full version.

If you want to move a project from Vijeo Designer to Vijeo Designer Basic, you can opt to:

-> Manually recreate the project in Vijeo Designer Basic.

-> Export assets (like images or text) from the original project where possible.

-> Rebuild screens and logic using the tools and features available in the Basic version.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)