המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the purpose for the 'ovs_att' PIDFF parameter.

The 'ovs_att' is the overshoot attenuation parameter of PIDFF block.  It is a tuning coefficient that can have a value between 0 and 1.  It can be used to  reduce overshoot when the setpoint changes.  The value is a user defined input.

  • A value equal to 1 provides the maximum attenuation.
  • A value equal to 0 provides no attenuation.

dfg

This can be used on a slow acting loop (i.e., temperature control, level control, etc.).  It is common to set it to an intermediate value (for example around 0.3–0.7 depending on the dynamics) and fine‑tune it empirically to obtain an acceptable compromise between speed and overshoot.