המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
In Vijeo Designer v6.3, what is the maximum number of client connections for VijeoViewer clients to an Harmony HMI's WebGate?

Issue

In Vijeo Designer v6.3, what is the maximum number of client connections for VijeoViewer clients to an Harmony HMI's WebGate?


Product Line

Vijeo Designer v6.3


Environment

VijeoViewer Tool running on Windows 10/11 PC or laptop connecting to physical HMI


Resolution

The maximum number of concurrent VijeoViewer client sessions that can be connected to a single Harmony HMI (running a project with WebGate configured) is 8.


Note: This is the same number of maximum connections as with Vijeo Designer v6.2.12 and older using Microsoft Edge (or Internet Explorer) as the client to a Harmony HMI running a project with WebGate configured.




If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)