Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many devices/registers can be IO scanned by 140CPU65160 Module, Modicon Quantum Range?

140CPU65160 can IO scan up to 128 devices/registers maximum.

The total number of input and output words which can be scanned during one cycle is 4000 each.
Note:
The maximum number of devices which can be used for IO scanning differs according to the type of module.
The attached table shows the IO scan limitation for Modicon Quantum range CPUs.

Schneider Electric India

Attachment(s)
1.jpg [105.62 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings