Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the frequency for Illuminated beacon reference XVBL8B4.
The Frequency of the illuminated Beacon unit,Red colour with 10 Joule “flash” discharge tube XVBL8B4 with 24VDC supply will depend on the temperature.
At 25°C and 55°C,below are the Frequencies Tolerance Ranges:
At 25°C    0.67Hertz< F < 2Hertz<==> 0.5seconds < T < 1.5seconds
At 55°C    0.5Hertz < F < 1.25Hertz <==> 0.8seconds < T < 2seconds
T- Time Period.
F-Frequency.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings