Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between tLIM and tLIG on Altivar 32 drive.
tLIM permit to limit the torque when the motor is in motor mode and tLIG permit to limit the torque when the motor is in
generator mode. So, these functions permit to limit the motor available torque (for example in case of motor mode, if torque
need by application increased more than the limit ,then the speed will decrease and the torque does not exceed the limit) ,and
not to stop the motor when the limit is reached.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings