Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to calculate the response value (C/K value) for a 6.6KV capacitor bank.
Normally the response value, more generally known as the C/K, is set automatically as a part of the Auto Setup sequence, but
there are cases when these values must be entered manually. The correct value can be calculated using an equation requiring
the 1st step size (in vars). Line-to-line voltage of the network used (in volts) and the CT ratio as follows;
C/K = (Q1st) / (I1/5A * ULL * 1.73)
Where Q1st = Size of 1st step in vars
ULL = line-to-line voltage in volts
I1/5A = CT ratio
For example: for a 100kvar step under 6.6 kV with a CT of 2000/5,
C/K = 0.022, the choice is 0.02 to be set into the controller.
Caution: when the customer can see on the display “Verify", you mustn’t validate this parameter and you must go out of the manual
setup sequence. When we do "manual setting", we never use "VERIFY".Because VERIFY checks all parameters (as an auto setting).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings