Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the value of making capacity (Icm-kA peak) for compact NSX range of circuit breaker.
According to the IEC60947-2, if the making capacity (Icm) is equal to the value specified in the attached file ,it is not
imperative to have a marking on the MCCB concerning the Icm value.
This is the reason why there is no information about the Icm concerning the marking and concerning the catalog.

Refer the snapshot-
As an example –
For the Compact NSX, the short circuit breaking capacity at 440V is 130KA, then Icm can be calculated by the
formula (as per attached IEC document)---
=> Icm = 2.2 x Icu = 2.2 X 130= 286 kA rms.

Schneider Electric India

Attachment(s)
servlet.jfif [122.33 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings