Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the RST Button on Advantys STB Island and what is the function of this button.
The RST button is located immediately above the CFG port, and behind the same hinged cover.
Holding down the RST button for 2 seconds or longer causes Flash memory to be overwritten, resulting
in a default configuration for the island.

If the island is already auto-configured, there is no consequence other than the island stops during the
configuration process. However, island parameters that you previously customized with the Advantys Configuration
Software are overwritten by default parameters during the configuration process.
Do not attempt to restart the island with the RST button. Pushing the RST button reconfigures the island with default settings.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings