Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is BUF (Braking Unit Fault) in Altivar 71 Drive.
This fault appears only for the drives > 90kW.
This fault appears when there is a short-circuit on the output of the braking transistor (desaturation of the braking IGBT).
Refer to attached file for more detail.

Schneider Electric India

Attachment(s)
ATV71_BUF fault.pdf [104.41 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings