Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum resetable & break time in Masterpact NT/NW and Easypact MVS control units.

Maximum resettable and maximum  break times are the times linked to instantaneous protection.

> Maximum resettable time is the time the breaker could withstand a fault before giving a tripping order. It means maximum resettable time is the time
during which a FAULT can appear, before the trip of the circuit breaker.

> Maximum break time is the maximum time for the Circuit breaker and the Micrologic to eliminate the fault. It means maximum break time it is the tripping
time including the global tripping chain of the circuit breaker.

The maximum resettable time is included in the maximum break time.

The maximum resettable time is 20ms where as the maximum break time is 50ms.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings