Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do enable the displaying of 2- and 3- phase measurement of BCPM in ION Enterprise 6 or Structureware Power Monitoring 7 Vista. 
The 2- and 3-phase measurements of BPCM are actually in the translator but which are "disable/hidden" by default.
To "enable/un-hide" it, you are required to edit the .ion file manually.
Right near the middle of the \system\translator\bcpm.ion file, there are two boolean registers defined that control whether the 2- and 3-phase measurements are shown
for bcpms: by default they have a value element set to false.
<t:V>false</t:V>
You must change the value to true as shown below:
<t:ION t:SA="ModuleObj" t:H="153092352" t:P="146" t:N="Two Phase Visible" t:CI="ExternalBoolean_Module">
<t:OH>
<t:ION t:SA="BoolObj" t:H="153092353" t:P="153092352" t:N="Two Phase Visible" t:CI="Boolean_Register">
<t:V>true</t:V>
</t:ION>
</t:OH>
</t:ION>
<t:ION t:SA="ModuleObj" t:H="153092608" t:P="146" t:N="Three Phase Visible" t:CI="ExternalBoolean_Module">
<t:OH>
<t:ION t:SA="BoolObj" t:H="153092609" t:P="153092608" t:N="Three Phase Visible" t:CI="Boolean_Register">
<t:V>true</t:V>
</t:ION>
</t:OH>
</t:ION>
After making the change & saving the file, re-start "ION Site Server" service for it to take effect. No extra device licenses are needed.
Regarding the Vista diagrams, unfortunately 2nd and 3rd phase measurements are not included in the default diagrams. Customers that wish to see these must add them into the diagram manually.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings