How can we help you today?

Can i format M340 CPU SD card using windows.

One can not format the M340 memory card with a non-Schneider tool. The memory card needs a structure to contain program and data. Formatting with another tool or windows destroys this structure. Also you should not use a write-protected memory card with the module. Some services do not operate properly when the memory card is write-protected.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings