Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the configuration of an Ethernet communication module ECC card stored in the meter or in the card itself
The configuration of the ECC (IP address, subnet mask, default gateway) is stored in the meter itself. If an existing meter with an ECC is replaced but still uses the original ethernet card, then the configuration will have to be set again in the new meter.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings