Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which version of Vijeo Designer I can configure HMIGXO panels and what is the procedure to add this GXO Series in my Vijeo Designer.
The minimum Version of Vijeo Designer to use GXO HMI version 6.0 Service Pack 2. If you are having the licensed version of Vijeo Designer V6.0 SP2 then only you can be able to add the GXO series of HMI in the software.
Upgrading the software is free of cost for HMI GXO series but only the thing is you need to have the License version of Vijeo Designer V6.0 SP2.
For this follow the procedure below:
1. In Vijeo Designer, click on the Help menu, then click on About.
2. In the dialog window, select the Licence tab, then click on the Upgrade button.
3. You may then put the upgrade reference number as VJDHTGTGX and press upgrade.
After that you can be able to view the GXO Series panels in your Vijeo Designer project configurations.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings