Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Quantum ERIO system how to increase length of RIO network more than 100 meters apart without using DRS (dual-ring switch)
Using 140 NRP 312 00/01 fiber converter modules in a Quantum EIO network allows you to transition from copper to fiber cable then back again to copper cable.
140 NRP 312 00/01 modules can be used to extend the distance between the local rack and an RIO drop, between 2 RIO drops, or between primary and standby racks in a Hot Standby system.
140 NRP 312 00/01 fiber converter modules have 2 copper ports and 2 fiber ports. The fiber ports, in both multi-mode and single-mode modules, use LC-type connectors. One fiber port is used as the transmitter signal (Tx), and the other fiber port is used as the receiver signal (Rx).

140 NRP 312 00/01 fiber converter modules are an alternative method to using a dual-ring switch (DRS) to provide fiber optic communications in a Quantum EIO system. You can install 140 NRP 312 00/01 modules on Quantum local and RIO drops to:
  • extend the total length of the Quantum EIO network (RIO drops in separate areas of a factory that are more than 100 m apart)
  • improve noise immunity
  • resolve possible grounding issues when using different grounding methods is required between 2 buildings
There are 2 models of fiber converter modules, each supporting one type of fiber cable:
  • 140 NRP 312 00 supports multi-mode fiber cable.
  • 140 NRP 312 01 supports single-mode fiber cable.

Do not connect a 140 NRP 312 01 single-mode fiber converter module to a 140 NRP 312 00 multi-mode fiber converter module.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings