Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is meaning of "bridge mode" in 140NOM2xx00 module
The 140 NOM 2xx 00 are modbus plus option modules which has modbus plus as well as a modbus connector on them. A bridge mode capability in the module permits a panel device connected to modbus port to access nodes on the Modbus Plus network or to access the local PLC directly without having to go out onto the network.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings