Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Maximum counting frequency of HSC (High speed counter) of SoMachine depend on any settings. If it depends what is it
Yes, maximum counting frequency of HSC of SoMachine depends on the set filter value of counting inputs
For one shot and Modulo loop mode of HSC Simple type, One shot mode of HSC Main type, Event counting mode of HSC Main type and Frequency meter mode of HSC Main type counter Pulse A is the counting pulse.
For this below is the relationship of Maximum counting frequency with Pulse A filter value
  • Maximum counter frequency is 100 KHZ if filter for counting input is set to 0.004 ms (default)
  • Counter frequency is 1 KHZ if filter for counting input is set to 0.4 ms
  • Counter frequency is 400 HZ if filter for counting input is set to 1.2 ms
  • Counter frequency is 100 HZ if filter for counting input is set to 4 ms
For Modulo loop mode of HSC Main type and Free large mode of HSC Main type counter pulses A and B are the counting pulses
For this below is the relationship of Maximum counting frequency with Pulse A and Pulse B filter value
  • Maximum counter frequency is 100 KHZ if filter for counting input is set to 0.004 ms (default)
  • Counter frequency is 1 KHZ if filter for counting input is set to 0.4 ms
  • Counter frequency is 400 HZ if filter for counting input is set to 1.2 ms
  • Counter frequency is 100 HZ if filter for counting input is set to 4 ms

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings