Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What kind of nuts and bolts are required for connecting busbars (Cu ETP-NFA51-100) to the Masterpact NW circuit breaker.
For connecting busbars (Cu ETP-NFA51-100) to the Masterpact NW circuit breaker it is recommended to use class 8.8 steel nut & bolts.
The tightening torques to be used while connecting busbars (Cu ETP-NFA51-100) to the Masterpact NW circuit breaker are shown in the table below:
The same torques can be used with AGS-T52 quality aluminium bars (French standard NFA 02-104 or American National Standard H-35-1).

Capture.JPG

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings