Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How I connect to STBNIP2212 if I forgot the IP
Use clear IP to clear the stored IP in the module by following below procedure.
The lower (ONES) switch is set to one of the CLEAR IP positions to clear both the NIM’s IP parameters and stored device name from Flash memory and no IP address is assigned. The module then waits for a new IP address assignment via available methods. Set the switches in accordance with your system and network requirements and repower the module.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings