Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the MTBF values for ABL8RPS24100 power supply.

MTBF will depends on the main power supply as these ABL8 power supplies may have the input voltage range from 100...120 V AC single phase [terminal(s): N-L1] or 200...500 V AC phase to phase [ terminal(s): L1-L2 ].

When working at 100% nominal load, MTBF of ABL8RPS24100 at 40°C ambient temperature is below :

At main power 220V: 33330 hours
At main power 500V : 29600 hours

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings