Yes, ACE850 has only one IP address used by both P1 and P2 port.
It is possible to use one port or two port depending on the network topology.
It is possible to use one port or two port depending on the network topology.
Released for: Schneider Electric India