Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Difference between TSXPSY2600 and TSXPSY2600M.

There is no difference in Hardware between TSXPSY2600 and TSXPSY2600M, physically both are same. Go through the meaning of the Last digit on the power supply module in catalog.
The various combinations mean new products  with the following rules:
- E means: product delivered with English documentation
- F means: product delivered with a french documentation
- M means: product delivered with multilingual documentation (E+F+...)
- No final letter means that the product has no associated documentation.

For Example
TSXPSY2600M = means TSXPSY2600 is supplied with multilingual documentation.
TSXPSY2600 = means TSXPSY2600 is supplied without any documentation.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings