Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the derating for high altitude application for Altivar 312 drive.
For ATV312H*****  Up to 1000 meter without derating.

For ATV312H***M2: Up to 2000 for single-phase supplies and corner grounded distribution networks,
derating the current by 1 % for each additional 100 m.

For ATV312H***M3, ATV312H***N4 & ATV312H***S6 : Up to 3000 metres for three-phase supplies, derating the current by 1 % for each additional 100 m.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings