Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the recommendations to select the Generator for Altivar 71 drive.
The generator must deliver the starting current with the minimum variation of the voltage frequency and drop voltage.

So, the power of the generators depends also on the acceleration ramp and the current limitation set in the ATV.

The current harmonics overheat the generator windings because the RMS current is higher compared to a sinus current. Because of that, a line choke is helpful.

Generally for the generator, 2 times the motor power is generally enough.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings