Password handling
The passwords can only be changed using VAMPSET software connected to the local RS-232 port on the relay.
It is possible to restore the password(s) in case the password is lost or forgotten. In order to restore the password(s), a relay
program is needed. The serial port settings are 38400 bps, 8 data bits, no parity and one stop bit. The bit rate is
configurable via the front panel.
Command Description
get pwd_break --> Get the break code (Example: 6569403)
get serno Get --> the serial number of the relay (Example: 12345)
Send both the numbers to country customer care center and ask for a password break. A device specific break code is sent back to you. That code will be valid for the next two weeks.
Command Description
set pwd_break=4435876 --> Restore the factory default passwords (“4435876” is just an example. The actual code should be asked from VAMP Ltd.)
Now the passwords are restored to the default values.
The passwords can only be changed using VAMPSET software connected to the local RS-232 port on the relay.
It is possible to restore the password(s) in case the password is lost or forgotten. In order to restore the password(s), a relay
program is needed. The serial port settings are 38400 bps, 8 data bits, no parity and one stop bit. The bit rate is
configurable via the front panel.
Command Description
get pwd_break --> Get the break code (Example: 6569403)
get serno Get --> the serial number of the relay (Example: 12345)
Send both the numbers to country customer care center and ask for a password break. A device specific break code is sent back to you. That code will be valid for the next two weeks.
Command Description
set pwd_break=4435876 --> Restore the factory default passwords (“4435876” is just an example. The actual code should be asked from VAMP Ltd.)
Now the passwords are restored to the default values.
Released for: Schneider Electric India


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.