Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum cable distance specified between Braking Unit and Braking resistor for Altivar 71 drive.
The potential problem of a very long resistor cable is to make an inductance. Then the switch of the resistor current could make some overvoltages to the transistor of the product.
On the other hand, the resistance of the cable could be higher than the braking resistor in such a case !
So, it is better to take care about the section of the cable to have a low resistance value.

However, It is possible to use up to 50 Meter Distance between Braking Unit and Braking resistor, but take care following:--
  • Need to take care about the cross section of the cable to have a low resistance value.
  • Also it is advise to use a shielded cable with 2 wire for assure the rule of EMC.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings