Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the response time to reach frequency reference on Altivar 71 drive.
Regarding response time of ATV71 drive, it depends on Acceleration time (ACC) and Rated motor freq. (FrS).

Example: if FrS =>50Hz and ACC =>60 Sec
Frequency reference => 50 Hz.
Then after run command, it will take 60 sec to reach 50Hz.

Example: if FrS =>50Hz and ACC =>60 Sec
Frequency reference => 30 Hz.
Then after run command, it will take 36 sec [(60x30)/50] to reach 30Hz.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings