Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is this possible that we get some other third party iPC or Standard PC that have an Windows Operating System then install Vijeo Designer Run time, will its work.
We have two reference numbers for Vijeo Designer Runtime software.

- For Magelis iPC (ref. VJDSNRTMPC)
- For Standard PC (ref. VJDSNRTSPC)

The reference VJDSNRTSPC is valid for Standard PC where Vijeo Runtime is to be installed (for example any PC or iPC other than Magelis iPC).

If you are using any Magelis iPC and looking for the Vijeo Runtime software the reference number would be VJDSNRTMPC. Please make sure that you have ordered the correct reference number according to your PC you will be given a serial number and license in order to get the software registered via the web. At the time of authorization, you will be asked to put the reference number and serial number for the product. After these steps, you will have to proceed with the registration wizard to complete the authorization.

In order to proceed with the registration steps without any problem please make sure to use the correct reference number of the Vijeo Runtime software.

Also please take note that Vijeo Designer Runtime registration is a one-time registration and is not transferable, which means it cannot be transferred from one PC to another PC. So at the time of registration, you will have to take care that you are registering the license on the correct PC.

You will have to take care of the supported Operating System by Vijeo Designer Runtime on the PC where you are going to install it.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings