Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
For Lexium 32 A / M drives, is it possible to have home position without performing reference movement of servo motor
Yes, it is possible. Set  Parameter  “HMmethod” =35. This means Homing by Position setting.

With this setting and triggering HOME command from fieldbus ( Lexium 32 A or M) , current position of servo motor will be regarded as Home position. Motor position at Home position can be defined with parameter “HMp_setP” parameter.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings