PARfactoryset = YES set all the parameters to default values and these saved to EEPROM.
PARuserrest = YES or bit 0 from Modbus or Fieldbus set all parameters to default values except
PARuserrest = YES or bit 0 from Modbus or Fieldbus set all parameters to default values except
- Communication parameters
- Inversion of direction of movement
- Selection of signal type for PTI interface
- Setting of encoder emulation
- Function of digital inputs / outputs
Released for: Schneider Electric India