Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum working temperature for motor choke VW3A5103.
Regarding motor Choke VW3 A5 103, the temperature of motor choke depends of the ambient temperature, motor current, PWM frequency etc….
Motor choke used on the condition specifies at catalog can works on the range (-10°C to 50°C).
The temperature of motor choke can increase at 50°C ambient up to 120 degree centigrade (worst case).

The thermal switch is advice to connect it for protecting itself and assure is longevity (and for not overheat it and burn it).
Trip in fault at 125°C by the thermal switch (Thermal protection by temperature-controlled switch).
Note: temperature-controlled switch contact should be connected in the sequence (controlling the line contactor).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings