It is a normal behavior of the M580 architecture that if user install the BMXXBE1000 extender module in the rack then they has to take care of below points else CPU will go in offline during self-test and not allow user to connect with it.
1. Remove power from all elements of the station (the local rack or remote drop) before inserting or extracting a line terminator.
2. If Extender module is installed then it should be properly connected with the cable or if unused port is there it should be terminated with TLY line terminator.
3. The unused ports on the 2 extender modules are terminated, with a TSX line terminator on the main rack and TLY line terminator on the extender rack .
Note:Pulling out rack expander cable while plc rack and in rack equipment's are online (powered ON state) is not recommended. Failure to follow this instruction can result in equipment damage.
1. Remove power from all elements of the station (the local rack or remote drop) before inserting or extracting a line terminator.
2. If Extender module is installed then it should be properly connected with the cable or if unused port is there it should be terminated with TLY line terminator.
3. The unused ports on the 2 extender modules are terminated, with a TSX line terminator on the main rack and TLY line terminator on the extender rack .
Note:Pulling out rack expander cable while plc rack and in rack equipment's are online (powered ON state) is not recommended. Failure to follow this instruction can result in equipment damage.
Released for: Schneider Electric India






Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.