Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In HMIGTO5310 , do we have any limit for the DRAM & SRAM for data storage, can we use this memory to log the data variable in HMI.
You can use DRAM & SRAM also to log your variable tag data but these DRAM & SRAM has some data storage limit like in HMIGTO5310
DRAM is 128 MB & SRAM 512 KB. Also the DRAM can`t hold data after power recycle but SRAM can hold data after power recycle.

If I conclude this then you can store data in DRAM & SRAM , but only SRAM will hold your data in case of any power failure and there would be
limit of 10 to 300 data records for SRAM while in DRAM you can store data records from 0 to 1000 per variable.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings