Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which cable we can use in order to connect SR2MOD3 DB9 connect to laptop DB9 connector using RS232 serial and pin details of the cable.
The SR2MOD03 modem has a SubD9 female connector to be connected on a RS232 serial link.
To connect this modem on the PC, it is necessary to use a standards RS232 extension cord with a side SubD9 Male and a side SubD9 Female.( it must be a pin to pin cable and all pin must be used). It is possible to use the cable SR1CBL03

This RS232 communication is Full Duplex type of communication.

Also this is a pin to pin cable that means (pin1 connected to pin1 , pin2 connected to pin2 ......pin9 to pin9 ).
This cable is SubD9 male at one end and SubD9 female at other end.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings