Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the causes of input current unbalance on ATV71 drive.
(1) Example: input current R=190, Y=215, B=216 at the input side of drive.
To know, if the problem comes from the ATV61 or from the main supply; this can be done if you inverse R and Y and perform the measurement of current. If the current in R becomes equal to 215 and the current in Y is 190, it means that the problem comes from the main supply.

(2) The balance of the current depends on the supply characteristics:
An unbalanced input current may be caused by an unbalanced main supply voltage. We say that the unbalance voltage do not exceed 1.8% of the nominal voltage. Please check it.

(3) Perhaps other devices are unbalanced or connected between two phases or phases and neutral.

(4) The input phase unbalance may be caused by a too small power for the main transformer. The transformer must be 2 times minimum the power of the drive.

(5) Make confirm cable size is same for all 3 phases, as impedance network can cause unbalance of phase input current.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings